Do I need to get an activation code for SoMachine V4.3 OPC UA?
Issue
Is a paid Activation ID or license required for OPC UA in SoMachine v4.3?

Product Line
SoMachine v4.3

Environment
PLC Configuration Software

Resolution
Prior to SoMachine V4.3 Patch 2, an activation code was required to get the OPC UA feature to be licensed and activated.
This activation code was provided through tech support at no additional cost.
With Patch 2 applied to SoMachine v4.3, the OPC UA  no longer requires an activation code.
SoMachine v4.3 Patch 2 is available through the Schneider Electric Software Update tool (SESU).

Note: The current iteration of SoMachine is now EcoStruxure Machine Expert v2.1

Schneider Electric Việt Nam

Tìm hiểu thêm
Phạm vi:
Bài viết có thể hữu ích
Tìm hiểu thêm
Phạm vi: