Does Vijeo Designer and EcoStruxure Operator Terminal Expert Runtime have the year 2038 limitation?

Article available in these languages: Tiếng Tây Ban Nha

Issue:
On a Mageils HMI running Vijeo Designer or EcoStruxure Operator Terminal Expert, the date can only go as far as December 31, 2038.

Product Line
Magelis HMI ranges, Harmony HMI ranges, Vijeo Designer, EcoStruxure Operator Terminal Expert

Resolution:
Since Vijeo Designer and EcoStruxure Operator Terminal Expert Runtime are currently both 32-Bit applications, they both will be affected by the year 2038 problem. That is, the date and time that the HMI can hold can only be upto the year 2038.

Schneider Electric Việt Nam

Tìm hiểu thêm
Phạm vi:
Bài viết có thể hữu ích
Tìm hiểu thêm
Phạm vi: