How to check power fan functionality on ATV630C16N4?
If power fan never rotates when ATV is in operation, the fan should be removed and tested first mechanically by hand to exclude bearing malfunction, then electrical test using external 48V DC.
Attached picture shows cable that connects fan with X22 connector on power board.
Pin 1 and 2 on X22 provides 48V DC for the fan (pin1 +, pin2 -). Pin 3 is dedicated for fan feedback.

Schneider Electric Việt Nam

Phần đính kèm
Fan cable.jpg [46.66 KB]
Tìm hiểu thêm
Phạm vi:
Bài viết có thể hữu ích
Tìm hiểu thêm
Phạm vi: