{}

Nhãn hiệu của chúng tôi

Impact-Company-Logo-English Black-01-177x54

Chào mừng bạn đến với Trang web của Schneider Electric

Chào mừng đến với trang web của chúng tôi.

Tìm các câu hỏi thường gặp

What can cause an InF1 or internal error 1 error on the ATV630 and ATV930 Process Drives?

Issue:
ATV630ATV930 internal error 1 troubleshooting

Product Line:
ATV630 and ATV930 Process drives

Environment:
All

Cause:
• Unknown drive rating
• Power range or Voltage range parameter out of range
• Communication between CMP6 and Brick interrupted.
• Incompatible power brick in the system (voltage range / power range)

Resolution:
Unknown drive rating
Principle:
During initialization sequence, the compatibility of the different
device components is verified. If an component doesn't mach to the hardware configuration the fault InF1 occurs.
Probable causes
• Unknown drive rating
• Power range or Voltage range parameter out of range
• Communication between CMP6 and Brick interrupted.
• Incompatible power brick in the system (voltage range / power range)
Remedies
• Check the power rating and the voltage of the power bricks.
• connect to the SoMove service section and use the "drive type recovery function" to set a valid configuration to the power board.
• check the high speed link communication cables in the CMP6 and the CMI1

Schneider Electric Việt Nam

Tìm hiểu thêm
Danh mục:
AC Drives and Soft Starters
Tìm hiểu thêm
Danh mục:
AC Drives and Soft Starters