How do we open a PDF file from the Vijeo Designer Runtime ?
If the HMI platform you are using has a Windows Operating System, you can create a script in Vijeo Designer to open a PDF from the inside of Vijeo Designer.

Ensure you have a PDF reader installed.

The following syntax works with Adobe Acrobat Reader and PDFXCView

Sys.createProcess("C:\\Program Files (x86)\\Adobe\\Acrobat Reader DC\\Reader\\AcroRd32.exe", "/A C:\\SEI_XBTGH_QRG.pdf");



Schneider Electric Việt Nam

Tìm hiểu thêm
Phạm vi:
Bài viết có thể hữu ích
Tìm hiểu thêm
Phạm vi: