Can I set up the 140CRA31908 with an M580 Hot Standby CPU as standalone and then add the redundancy later without interruption?
Yes. This can be set up in a standalone configuration using a BMEH58x040 and then the other half can be added without interrupting the process.

If this FAQ did not solve your issue, you can chat with us at chat with us or e-mail us at customer.services@se.com to create a case with our Technical Support Team.

If you are not located in North America, please contact your local Customer Care Center for assistance:
Support | Schneider Electric Global (se.com)

Schneider Electric Việt Nam

Tìm hiểu thêm
Phạm vi:
Bài viết có thể hữu ích
Tìm hiểu thêm
Phạm vi: