Can the firmware version of X80 IO modules be accessed from the M580?

Issue
Trying to read the firmware version of Analog and Discrete IO modules using either Unity Pro or DDTs from the M580.

Product line
M580, X80, Unity Pro, Unity Loader

Resolution
There are no means for acquiring the firmware version of the IO modules from either the DDTs or Unity Pro. The only method of querying the firmware version of IO modules is using Unity Loader.

Schneider Electric Việt Nam

Tìm hiểu thêm
Phạm vi:
Tìm hiểu thêm
Phạm vi: