Product Line
PME 9.0
ION meter
Powerlogic meter
Environment
Resolution
Item | Details |
PM8000 Modbus/ION coexistence | PME 9.0 supports ION over Modbus communications with PM8000 (v1.4.1+) devices. |
ION9000 support | PME now supports the new high end ION9000 power monitoring device. |
New device type support | The following device types are now supported in PME 9.0 :
|
Updated device license requirements | PM8000 and MTZ now require a DL-S license (was DL-M before) |
For the list of default supported devices, please refer to FA363561
For more information, please refer to PME 9.0 documentation FA358303
Đã phát hành cho:Schneider Electric Việt Nam