What are the part numbers for the fan kit of ATV340 drives?
Issue:
Needs the part numbers for the fan kit of ATV340 drives

Product Line:
ATV340, Altivar 340 Altivar Machine

Environment:
All

Cause:
Replacing the heatsink fan.

Resolution:

ATV340U07N4 to ATV340U40N4, Size 1 = VX5VMS1001
ATV340U07N4E to ATV340U40N4E, Size 1 = VX5VMS1001
ATV340U55N4 to ATV340U75N4, Size 2 = VX5VMS2001
ATV340U55N4E to ATV340U75N4E, Size 2 = VX5VMS2001
ATV340D11N4 to ATV340D22N4, Size 3 = VX5VMS3001
ATV340D11N4E to ATV340D22N4E, Size 3 = VX5VMS3001


Instruction manual for the fans is attached.

Schneider Electric Việt Nam

Phần đính kèm
ATV340 fans NVE61755.pdf [2.49 MB]
Tìm hiểu thêm
Sản phẩm:
Bài viết có thể hữu ích
Tìm hiểu thêm
Sản phẩm: