SmartConnect Device Registration when QR Label is Missing
Problem: The label containing the QR code and Product ID and Product Key required to pair a new SmartConnect-enabled UPS to a SmartConnect portal account may appear to be missing. How can a SmartConnect-enabled device be registered without the SmartConnect label?

Product Line: SmartConnect enabled Smart-UPS:
SMT750IC, SMT1000IC, SMT1500IC, SMT2200IC, SMT3000IC, SMT1000RMI2UC, SMT1500RMI2UC, SMT2200RMI2UC, SMT3000RMI2UC;
SMT750C, SMT1000C, SMT1500C, SMT2200C, SMT3000C, SMT1000RM2UC, SMT1500RM2UC, SMT2200RMI2UC, SMT3000RM2UC;
SMC1000IC, SMC1500IC, SMC1000I-2UC, SMC1500I-2UC;
SMC1000C, SMC1500C, SMC1000-2UC, SMC1500-2UC;

Resolution:
Rack-mount UPS models may have the QR label attached to the front or rear panel of the unit rather than to the top - please inspect the rear and front panels.
Tower models have the QR label attached to the top of the UPS.
The Product ID and Product Key are printed on the QR label.

If the label is not available on the top, front or rear panel of the UPS, manual registration is possible.

1. For SMC models, please contact your local APC Tech Support and have the following information ready:
a) UPS model and serial number
b) photos showing the top, rear and front panels of the UPS

2. SMT UPS models can be paired to a SmartConnect portal account without the QR label. In order to identify the Product ID and Product Key references required for pairing:
a) using the UPS LCD Display, navigate to "About" menu and scroll to the "UPS MAC" and "Product Key" entries
b) log into your SmartConnect account and choose "ADD DEVICE" then "Product Codes", and input the codes identified on the UPS LCD:

img

img

Schneider Electric Việt Nam

Tìm hiểu thêm
Phạm vi:
Bài viết có thể hữu ích
Tìm hiểu thêm
Phạm vi: