What Broadcast Storm Protection settings are available in the Tesys T LTMR product?
Issue:
What Broadcast Storm Protection settings are available in the Tesys T motor controller?

Product Line:
Tesys T, LTMR products.

Environment:
All models, All serial numbers

Cause:
Clarification of capabilities.

Resolution:
The LTMR product have Broadcast Storm Protection enabled by default at 1000 kbps bandwidth.   This can be changed via Modbus/TCP register 3104 (Ethernet IP Object address 96 : 01 : 69).  There are six possible settings for this parameter:

0 : Disabled
1 : 64 kbps bandwidth
2 : 128 kbps bandwidth
3 : 256 kbps bandwidth
4 : 512 kbps bandwidth
5 : 1000 kbps bandwidth (factory default)

Schneider Electric Việt Nam

Tìm hiểu thêm
Phạm vi:
Bài viết có thể hữu ích
Tìm hiểu thêm
Phạm vi: