Can the side doors or rear fan panels of the NetShelter CX/CX2 be secured with the NetBotz HID door handle? If not, is there a more secure option?
Issue:
I customer is looking to make the side door more secure, thus making access to the rear fan panels more secure.

Product Line:
NetShelter CX

Environment:
All models and serial ranges.

Cause:
The customer cannot find options to make the rear fan trays more secure.

Resolution:

Currently there is no way to increase security to accessing the rear fan units or side doors. The HID door handle solution available for the front door cannot be implimented on the side or rear.

Schneider Electric Việt Nam

Tìm hiểu thêm
Phạm vi:
Bài viết có thể hữu ích
Tìm hiểu thêm
Phạm vi: