Do the iEM3000 meters support Demand calculations?
Issue
Do the iEM3000 meters support Demand calculations?

Product Line
Acti 9 iEM3000 (iEM3455, iEM3465, iEM3555, iEM3565)

Environment
Meter technical specifications

Resolution
Demand Readings are available in the iEM34xx and iEM35xx models from the below firmware versions. iEM34xx and iEM35xx models with older firmware
versions cannot be upgraded.

• iEM34x5 - V1.2.003 and higher
• iEM35x5 - V1.1.001 and higher
• iEM3465 and iEM3565 - BACnet V2.4 and higher

Demand registers are listed in the latest iEM3000 Series User Manual available at the iEM3000 Documents & Downloads page.

Schneider Electric Việt Nam

Tìm hiểu thêm
Phạm vi:
Bài viết có thể hữu ích
Tìm hiểu thêm
Phạm vi: