What is the required control voltage for the ATS48?
Issue:
Required control voltage for the ATS48.

Product Line:
Altistart 48 Soft Starter

Environment:
All

Cause:
Installation documentation

Resolution:
ATS48...Q the control circuit voltage is 220 - 15 % to 415 + 10 %, 50 / 60 Hz
ATS48..Y control circuit voltage is 110 - 15 % to 230 + 10 %, 50 / 60 Hz
This is AC voltage, and is applied to the CL1 and CL2 terminals.

Electrical Characteristics

Schneider Electric Việt Nam

Phần đính kèm
ATS48 wiring.pdf [69.85 KB]
Tìm hiểu thêm
Phạm vi:
Bài viết có thể hữu ích
Tìm hiểu thêm
Phạm vi: