How do I connect an HMIDM Modular Display touch-screen to a PC as a monitor?
Issue
How do I connect an HMIDM Modular Display touch-screen to a PC as a monitor?
The panel does not seem to have a DVI, DisplayPort, or HDMI socket built into it.

Product Line
Magelis HMIDM Modular Display (HMIDM7421, HMIDM7521, HMIDM9521, HMIDMA521, HMIDM6421, HMIDM6521)
Magelis Modular Box PC

Resolution
The Magelis HMIDM Modular Display touch-screens  do not have DVI, DisplayPort, or HDMI sockets built into them. They are designed to be connected directly to Magelis HMIBM Modular Box PC CPU/Motherboard modules via a proprietary connector for display.

To connect this line of Modular Display via Display Port to a PC, a display adapter with Reference Part Number HMIDADP11 must be purchased.
https://www.se.com/ww/en/product/HMIDADP11/display-adaptor-dp-for-hmidm/

Note: The HMIDADP11 can also display video to a Magelis Modular Display from a Magelis HMIBM Modular Box PC via Ethernet remotely.

If the PC does not have a DisplayPort video output, DVI output from the PC can be converted with a DVI to DisplayPort adapter with Reference Part Number HMIYADDPDVI11.
https://www.se.com/us/en/product/HMIYADDPDVI11/adaptor-from-display-port-to-dvi-d/

Schneider Electric Việt Nam

Tìm hiểu thêm
Phạm vi:
Bài viết có thể hữu ích
Tìm hiểu thêm
Phạm vi: