Where can I find braking unit and braking resistor part numbers for ATV9xx Process Drives?
Issue:
ATV9xx Process Drives braking unit part number

Product Line:
Altivar 930

Environment:
All

Cause:
Braking unit part numbers needed

Resolution:
Part numbers for braking units and braking resistors for ATV900 drives can be found in the attached document, which is an excerpt from the ATV900 Catalog.
Pricing & availability can be obtained from your local distributor and Customer Service.

Note: These braking units and resistors are for ATV900 series Process Drives only. The ATV600 series cannot be wired for a braking resistor.

Schneider Electric Việt Nam

Phần đính kèm
ATV900 DB resistors.pdf [1.51 MB]
Tìm hiểu thêm
Phạm vi:
Bài viết có thể hữu ích
Tìm hiểu thêm
Phạm vi: