Issue:
How can an ATS48 be connected to and configured with SoMove?
Product Line:
Altistart 48
Environment:
All
Cause:
ATS48 Soft Starters can be configured with SoMove
Resolution:
1) Download the latest version of SoMove FDT here:
https://www.se.com/en/download/document/SoMove_FDT/
2) Download the latest version of Altistart DTM here:
https://www.se.com/en/download/document/Altistart_DTM_Library/
3) To connect the Altistart to your computer (RJ45/USB),
you need to order the Schneider Electric Modbus Serial Cable (RJ45/USB), code = TCSMCNAM3M002P
https://www.se.com/en/product/TCSMCNAM3M002P/
4) watch the video
Đã phát hành cho:Schneider Electric Việt Nam