Video Altivar: How to set BACnet communication in ATV212 using SoMove?



Issue:
Setting up Bacnet communication in a ATV212, with Somove

Product Line:
ATV212

Environment:
SoMove

Cause:
n/a

Resolution:
1) Download the latest version of SoMove FDT here:
https://www.se.com/en/download/document/SoMove_FDT/

2) Download the latest version of Altivar DTM here:
https://www.se.com/ww/en/download/document/Altivar_DTM_Library/

3) To connect the ATV212 to your computer (RJ45/USB),
you need to order the Schneider Electric Modbus Serial Cable (RJ45/USB), code = TCSMCNAM3M002P
https://www.se.com/en/product/TCSMCNAM3M002P/

4) watch the video to set BACnet

Schneider Electric Việt Nam

Tìm hiểu thêm
Phạm vi:
Bài viết có thể hữu ích
Tìm hiểu thêm
Phạm vi: