What do the LED indicators on the ATV340 drives mean?

Issue:
Meaning of the LED on ATV340

Product line:
ATV340

Environment:
All models, all serial numbers.

Cause:
Clarification of product features.

Resolution:
There are two sets of LEDs available, depending on the part number of the drive.  See the diagrams below for details:



Schneider Electric Việt Nam

Phần đính kèm

ATV340 LEDs 1.PNG.pngATV340 LEDs 1.PNG.png [33.46 KB]
ATV340 LEDS 2.PNG.pngATV340 LEDS 2.PNG.png [56.98 KB]
ATV340 LEDs 3.pngATV340 LEDs 3.png [22.6 KB]
Tìm hiểu thêm
Phạm vi:
Tìm hiểu thêm
Phạm vi: