How many cables can be connected to the 04456 connection plate?

The distance between two consecutive connection plates on the 04456 is 64 / 65mm:

Each connection plate is prepared for the connection of maximum 8 cables (4 on each face of a connector plate).


It's the responsibility of the panel builder and sub-contractor to check creepage distance and more specifically clearance distance of connections on the connector plates: see IEC61439-1, for Ui =1000V the clearance distance must be greater or equal to 14 mm.

Schneider Electric Việt Nam

Tìm hiểu thêm
Phạm vi:
Tìm hiểu thêm
Phạm vi: