On an ATV212, can the analog input be programmed for 0-10V to control 30-60Hz?
Issue:
Programming analog input for 0-10V to control 30-60 Hz on an ATV212 Drive.

Product Line:
Altivar 212

Environment:
All

Cause:
Wants 0-10V to equal 30-60Hz

Resolution:
Yes, this is accomplished by adjusting the scaling of the applicable analog input so that the drive knows that 0%=30Hz.

If you're using VIA: Adjust F201 to 0%, F202 to 30Hz, F203 to 100% and F204 to 60 Hz.
If you're using VIB: Adjust F210 to 0%, F211 to 30Hz, F212 to 100% and F213 to 60 Hz.

For details on accessing these parameters please see the FAQ on ATV212 Basic Programming.

Schneider Electric Việt Nam

Tìm hiểu thêm
Phạm vi:
Bài viết có thể hữu ích
Tìm hiểu thêm
Phạm vi: