What can cause an INFb [Internal Error 11] fault on an ATV340 series drive and how do i correct it?
Issue:
Customer is experiencing an INFb [Internal Error 11] fault on an ATV340 series drive.

Product Line:
ATV340

Environment:
All

Cause:
The internal drive thermal sensor is not operating correctly.

Resolution:
Cycle power to clear the fault.  If the fault returns, contact your local Schneider Electric representative.

Schneider Electric Việt Nam

Tìm hiểu thêm
Phạm vi:
Bài viết có thể hữu ích
Tìm hiểu thêm
Phạm vi: