undefined undefined
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
How do you program a relay on the ATV630 to close at speed reached

Article available in these languages: Tiếng Tây Ban Nha

Issue:
Customer wants to have R1 close when motor frequency reaches the reference frequency.

Product Line:
Altivar ATV600 and ATV900

Environment:
All serial numbers

Cause:
Customer set up R1 frequency reference attained.

Resolution:
Check R1 assignment under Complete Settings -> Input/output -> Relay -> R1 Configuration -> R1 assignment ->  [Ref Freq Reached] SrA or Frequency reference reached.
R1A and R1C will close at and above Frequency reference.

Schneider Electric Việt Nam

Tìm hiểu thêm
Phạm vi:
Bài viết có thể hữu ích
Tìm hiểu thêm
Phạm vi: