What is the NSYAEFPFPTD accessory to the NSYPTDS* flange kit?
Issue:
NSYAEFPFPTD accessory in the NSYPTDS* flange kit.

Product Line:
Process drives

Environment:
N/A

Cause:
Option or required?

Resolution:
When a Process drive is flange mounted into a wall mounted enclosure, the heatsink extends out the back.  Space is required between the enclosure and wall to accommodate the heatsink and airflow.  The NSYAEFPFPTD is a bracket kit to extend the enclosure away from the wall.  The bracket can provide the space for the NSYPTDS1, NSYPTDS2, and NSYPTDS3 flanged drives.
See the attached file.

Schneider Electric Việt Nam

Phần đính kèm
Flange mtd brkt NSYAEFPFPTD NHA3487201_00 Process.pdf [411.19 KB]
Tìm hiểu thêm
Phạm vi:
Bài viết có thể hữu ích
Tìm hiểu thêm
Phạm vi: