Ethernet IP Add-On-Profile for Altivar Process drives
Issue:
Is there an Add-on Profile available for Altivar Process Drives and Ethernet IP?

Product Line:
ATV630, ATV930

Environment:
All

Cause:
NA

Resolution:
There is no dedicated Add-On Profile (AOP) available for the Altivar Process series drives.
We only provide the EDS file to integrate the drive inside Rockwell PLCs.

Schneider Electric Việt Nam

Tìm hiểu thêm
Phạm vi:
Bài viết có thể hữu ích
Tìm hiểu thêm
Phạm vi: