Tìm các câu hỏi thường gặp
Does the ATV320 have 2 ramps functionality?
Issue:
Availability of Dual ramps with the ATV320 drives.
Product Line:
ATV320
Environment:
All serial numbers
Cause:
Application requirement
Resolution:
Yes, There is a second acceleration ramp option, ACC2 (ranges from 0.00 - 6,000 seconds)
![2 ramp functionality 2 ramp functionality](https://ckm-content.se.com/ckmContent/servlet/servlet.ImageServer?id=0158V00000EELGkQAP&oid=00DA0000000abSmMAI)
Availability of Dual ramps with the ATV320 drives.
Product Line:
ATV320
Environment:
All serial numbers
Cause:
Application requirement
Resolution:
Yes, There is a second acceleration ramp option, ACC2 (ranges from 0.00 - 6,000 seconds)
Đã phát hành cho:Schneider Electric Việt Nam
Tìm hiểu thêm
Phạm vi:
Tìm hiểu thêm
Phạm vi: