Tìm các câu hỏi thường gặp
How is the ATV212 set for RUN/STOP on the terminals and speed reference from the keypad UP/DOWN arrows?
Issue:
Trying to set the ATV212 for RUN/STOP on the terminals and UP/DOWN arrows for the speed reference.
Product Line:
Altivar Machines, Altivar 212
Environment:
All models and serial numbers
Cause:
Customer needs to use terminals for Start/Stop and Arrows on the faceplate of drive for speed reference
Resolution:
Set CNOD = 0 for terminals Start/Stop control.
Set FNOD = 3 for keypad UP/DOWN arrow button speed control.
Trying to set the ATV212 for RUN/STOP on the terminals and UP/DOWN arrows for the speed reference.
Product Line:
Altivar Machines, Altivar 212
Environment:
All models and serial numbers
Cause:
Customer needs to use terminals for Start/Stop and Arrows on the faceplate of drive for speed reference
Resolution:
Set CNOD = 0 for terminals Start/Stop control.
Set FNOD = 3 for keypad UP/DOWN arrow button speed control.
Đã phát hành cho:Schneider Electric Việt Nam
Tìm hiểu thêm
Phạm vi:
Tìm hiểu thêm
Phạm vi: