What is the manufacturer statement of compliance for IEEE 519 on S-Flex?
Issue:
Manufacturer statement of compliance for IEEE 519 on S-Flex.

Product Line:
Altivar 212 S-Flex

Environment:
All models

Cause:
Customer requests the manufacturer statement of compliance for IEEE 519 on S-Flex

Resolution:
The standard IEEE 519 is not related to a product, such as an Altivar drive, it’s related the quality of distribution networks.

ATV212 has a THDi less than 35%. It means, by itself, it will not comply with IEEE 519.
One solution to have a lower THDi is to use active filter such as AccuSine with an additional line choke. With this association (AccuSine + line choke + ATV212), THDi will be below 5%

But, without knowing the network characteristic (see picture below), we can’t make statement that ATV212 with the AccuSine and the line choke complies with IEEE 519.

Schneider Electric Việt Nam

Phần đính kèm
rtaImage.jpg [58.17 KB]
Tìm hiểu thêm
Phạm vi:
Bài viết có thể hữu ích
Tìm hiểu thêm
Phạm vi: