In need of none or odd parity setting on the Link150 when Modbus ASCII is used

Issue:

The user may require a specific parity setting on the Link150 (EGX150) when the transmission mode has been set to Modbus ASCII

Product Line:

Link150 (EGX150)

Resolution:

When the transmission mode is set to Modbus ASCII, the parity of the serial port is limited to EVEN. Unfortunately, parity cannot be adjusted to none or odd.

Schneider Electric Việt Nam

Tìm hiểu thêm
Phạm vi:
Bài viết có thể hữu ích
Tìm hiểu thêm
Phạm vi: