How to convert bits to an Integer in Vijeo Designer?
Issue:
Looking for a script method to convert bits to an Integer in Vijeo Designer?

Product Line:
Vijeo Designer (all versions)

Resolution:
To convert bits to be used an Integer variable in Vijeo Designer, please use a script as shown below:

boolean bitArray[] = new boolean[16];

int value = 0;

bitArray[0] = true;
bitArray[1] = true;
bitArray[2] = true;
bitArray[3] = true;
bitArray[4] = true;
bitArray[5] = true;
bitArray[6] = true;
bitArray[7] = true;
bitArray[8] = false;
bitArray[9] = false;
bitArray[10] = false;
bitArray[11] = false;
bitArray[12] = false;
bitArray[13] = false;
bitArray[14] = false;
bitArray[15] = false;

for (int i = 0; i < 16; i++)
{
if (bitArray[i])
{
value += 1 << i;
}
}

//TestINT is a Vijeo Designer INT variable that I created. This was just used to test the output.
TestINT.write(value);

Schneider Electric Việt Nam

Tìm hiểu thêm
Phạm vi:
Bài viết có thể hữu ích
Tìm hiểu thêm
Phạm vi: