Where is the project location for Vijeo Designer Runtime?
Issue:
Where is the project location for Vijeo Designer Runtime?

Product Line:
IPC, Generic PC, Vijeo Designer Runtime

Resolution:
The Vijeo Designer Runtime application is stored at <drive location set for user application>:\Program Files\Schneider Electric\Vijeo-Designer 6.2\Vijeo-Runtime\Public\Projects\

This is the location where the project is loaded from when the Runtime launches.

Schneider Electric Việt Nam

Tìm hiểu thêm
Phạm vi:
Bài viết có thể hữu ích
Tìm hiểu thêm
Phạm vi: