What is the recommended cable type to be used with the ATV660 drives?

Article available in these languages: Tiếng Tây Ban Nha

Issue:
Customer wants to know if they should use 2000V cables or 1000V/600V cables for long cable distances.

Product line:
Altivar Process, ATV630, ATV930

Environment:
All model numbers

Cause:
Long motor cable distance

Resolution:
The type of cable used depends on the length of the cable and the motor selection.
Each type or brand of wire will have different characteristics (insulation, coupling capacitance, etc).
Consult the cable manufacturer for selection recommendations.

Schneider Electric Việt Nam

Tìm hiểu thêm
Phạm vi:
Bài viết có thể hữu ích
Tìm hiểu thêm
Phạm vi: