Why I have some difficulties to connect to GateManager or LinkManager?
Issue
The GateManager version 8.3.19081 may have some compatibility issues with the browsers Internet Explorer 11 (IE11) and Mozilla Firefox.  These are experienced using the GateManager and LinkManager user interfaces.

Product Line
Offer impacted: Ecostruxure Secure Connect Advisor
Version of GateManager: 8.3.19081

Environment
Internet Explorer 11 (IE11) and Mozilla Firefox

Resolution
As a workaround, use another browser internet as Chrome

Schneider Electric Việt Nam

Tìm hiểu thêm
Phạm vi:
Bài viết có thể hữu ích
Tìm hiểu thêm
Phạm vi: