What is the center-to-center dimension of the square holes on the NetShelter VX Seismic side brace?
Issue:
The manual does not state the dimensions of the holes on the side braces that are used to set the mounting rail depth.

Product Line:
NetShelter XV Seismic

Environment:
All versions and serial ranges.

Cause:
The hole to hole dimension is needed check horizontal mobility of the mounting rails in the cabinet.

Resolution:

The dimension of the square holes in the side brace is 31.75mm center to center.
The holes are 9.5mm square.

Schneider Electric Việt Nam

Tìm hiểu thêm
Phạm vi:
Bài viết có thể hữu ích
Tìm hiểu thêm
Phạm vi: