PowerChute cannot be installed on 32-bit systems
Issue:
PowerChute cannot be installed on 32-bit systems.

Product Line:
PowerChute Business Edition
PowerChute Serial Shutdown
PowerChute Network Shutdown

Environment:
All supported OS

Cause:
  1. PowerChute Serial Shutdown is a 64-bit-only application.
  2. PowerChute Business Edition v10.0 and above are 64-bit-only applications.
  3. PowerChute Network Shutdown v4.3 and above are 64-bit-only applications.

Solution:
We no longer support 32-bit operating systems. To run PowerChute, upgrade the hardware to 64-bit.

Schneider Electric Việt Nam

Tìm hiểu thêm
Phạm vi:
Bài viết có thể hữu ích
Tìm hiểu thêm
Phạm vi: