What is the pickup voltage for the RSB series relays?

Issue:
Voltage at which the coil will engage

Product line:
Relays and Timers

Environment:
RSB Zelio Plug in Relays

Cause:
Documents show drop out voltage not pick up voltage

Resolution:
The pickup up voltage is within 70% of the rated coil voltage.

So for example on RSB1A120ED with a 48VDC coil, the pick up voltage is 33.6VDC.

Schneider Electric Việt Nam

Tìm hiểu thêm
Phạm vi:
Tìm hiểu thêm
Phạm vi: