What is the speed regulation / accuracy of the ATV320?
Issue:
Needs to know the speed regulation or accuracy of the ATV320 drive

Product Line:
ATV320

Environment:
All

Cause:
Speed regulation , accuracy

Resolution:

ATV320:
- Open loop
Speed range: 1:100
Speed accuracy: 10% of nominal slip
Torque accuracy: 15%

Schneider Electric Việt Nam

Tìm hiểu thêm
Phạm vi:
Bài viết có thể hữu ích
Tìm hiểu thêm
Phạm vi: