What is the latest version of SoMachine Motion?

Issue
Is there a version of SoMachine Motion newer than v4.4.1? If so, what is the latest version?

Product Line
SoMachine Motion, EcoStruxure Machine Expert

Environment
PLC/PAC Configuration Software for Windows

Resolution
SoMachine Motion v4.4.1 is the last version of SoMachine Motion.
SoMachine Motion v4.4.1 and SoMachine v4.3 devices have now been integrated into the single configuration software tool called EcoStruxure Machine Expert.
As of October 2023, The current version is EcoStruxure Machine Expert v2.1 with the Professional License. Use the Machine Expert Installer tool to customize your installation to add Motion Controllers.

Schneider Electric Việt Nam

Tìm hiểu thêm
Phạm vi:
Tìm hiểu thêm
Phạm vi: