Does EcoStruxure Machine Expert support M258, LMC058 and LMC078 controllers?

Article available in these languages: Tiếng Tây Ban Nha

Issue:
Some older versions of EcoStruxure Machine Expert versions do not have M258, LMC058 and LMC078 controllers on the list of available devices

Product Line:
M258, LMC058 and LMC078 controllers

Environment:
EcoStruxure Machine Expert versions 1.1, 1.2.x and 2.0 (formally known as SoMachine)

Resolution:
- EcoStruxure Machine Expert supports M258 and LMC058 controllers starting with version 1.2.5. Previous version of EcoStruxure Machine Expert did not support them.
- LMC078 controllers are not supported by any version of EcoStruxure Machine Expert. SoMachine 4.3 software should be used instead to program a LMC078 controller.
- EcoStruxure Machine Expert v2.0 will not support M258, LMC058 or LMC078 controllers anymore.

If this FAQ did not solve your issue, you can chat with us at chat with us or e-mail us at customer.services@se.com to create a case with our Technical Support Team.

If you are not located in North America, please contact your local Customer Care Center for assistance:
Support | Schneider Electric Global (se.com)

Schneider Electric Việt Nam

Tìm hiểu thêm
Phạm vi:
Bài viết có thể hữu ích
Tìm hiểu thêm
Phạm vi: