Is Control Expert compatible with Windows 10?
Issue
There is a need to use Control Expert V14 or V15 on a Windows 10 platform.

Product line
Control Expert

Resolution
As of 3/16/2022 all versions of Control Expert are supported on both Windows 10 32-bit and 64-bit operating systems.
If working with M580 products and or DTMs, 64-bit Windows is mandatory.


If this FAQ did not solve your issue, you can chat with us at chat with us or e-mail us at customer.services@se.com to create a case with our Technical Support Team.

If you are not located in North America, please contact your local Customer Care Center for assistance:
Support | Schneider Electric Global (se.com)

Schneider Electric Việt Nam

Tìm hiểu thêm
Phạm vi:
Bài viết có thể hữu ích
Tìm hiểu thêm
Phạm vi: