What are the technical details of the integrated optical transceiver of TCSESPU093F2CU0?
Issue
The TCSESPU093F2CU0 has two Multimode ports (type 50/125) and this FAQ gives the technical details of the integrated optical transceiver.

Product Line
ConneXium Switch

Environment
TCSESPU093F2CU0

Resolution
The TCSESPU093F2CU0 integrated optical transceiver has:
  • Maximum optical power: -14dBm
  • Transmit power: -23.5dBm
  • Receiver sensitivity: -31dBm
  • Loss budget: 7.5dBm

Schneider Electric Việt Nam

Tìm hiểu thêm
Phạm vi:
Bài viết có thể hữu ích
Tìm hiểu thêm
Phạm vi: