Control Expert on a VM: Trial version license expires before allotted time.
If the VM folder or properties change or the HOST ID changes, the Trial License is no longer valid.
The License  Server sees the change as a violation.

Control Expert would have to be loaded on a different VM.


Control Expert V14 has been successfully tested in the following configuration :
  • VirtualBox 5.1.30 r118389 and 5.2.0-118431
  • VMware Workstation 12 Pro 12.1.0 build-3272444

Schneider Electric Việt Nam

Tìm hiểu thêm
Phạm vi:
Bài viết có thể hữu ích
Tìm hiểu thêm
Phạm vi: