Why is my custom library missing after upgrading from Unity Pro to Control Expert?
Issue
After the migration to Control Expert the custom libraries that were installed with Unity Pro are no longer available.

Product line
Control Expert, Unity Pro

Resolution
After installation of Control Expert V14, the custom libraries from Unity Pro are still available in the initial installation directory C:\Documents and Settings\All Users\Application Data\Schneider Electric\Unity Pro\CustomLibset\Vx.y

This directory is not modified by Control Expert installation.

By default and whatever the version of standard library used, all applications will use the custom library located in the new directory created by Control Expert: \Documents and Settings\All Users\Application Data\Schneider Electric\Control Expert x.y\CustomLibset\Vx.y.

After Control Expert installation, the custom libraries from Unity Pro must be restored manually in the new default directory created by Control Expert

You can create a new custom library dedicated to previous versions of Unity Pro, by selecting the "custom library path": C:\Documents and Settings\All Users\Application Data\Schneider Electric\Unity Pro\CustomLibset\Vx.y in menu Tools/Options/General/Path.

When using Type library update tool, you have to select the right library path according to the path selected in the Options.


If this FAQ did not solve your issue, you can chat with us at chat with us or e-mail us at customer.services@se.com to create a case with our Technical Support Team.

If you are not located in North America, please contact your local Customer Care Center for assistance:
Support | Schneider Electric Global (se.com)

Schneider Electric Việt Nam

Tìm hiểu thêm
Phạm vi:
Bài viết có thể hữu ích
Tìm hiểu thêm
Phạm vi: