Do Vijeo Designer Events have an Active state?
Issue:
When setting the "Alarm & Event List" to Active for an Event Group, nothing is display during runtime when there are Events. The only settings that display Events are History and Log.

Product Line:
Vijeo Designer (all versions)

Resolution:
Events in Vijeo Designer have no concept of "state". In essence, an event is something that has occurred already in the past. Therefore is no such thing as an Active event in Vijeo Designer. When using the Alarm & Event summary, the setting "Alarm & Event List" can only be set to History or Log for Events. If monitoring states is required, it is recommended to use Alarms rather than Events.

Schneider Electric Việt Nam

Tìm hiểu thêm
Phạm vi:
Bài viết có thể hữu ích
Tìm hiểu thêm
Phạm vi: