EcoStruxure Machine Expert - Missing license feature EME_ProjectArchive message when opening a projectarchive file
Issue
When I try to open a .projectarchive file in EcoStruxure Machine Expert v1.1 or 1.2 I see the message:
"The command "Extract Archive…" could not be executed,
because you don't have the appropriate license on this PC.
Missing license feature: EME_ProjectArchive
Would you like to launch the 'Manage licenses' dialog to
Activate a license?"


How do I resolve this so I can open my project?

Product Line
EcoStruxure Machine Expert v1.1 or v1.2

Environment
PLC configuration software in Windows

Cause
The cause of this message is because the product is either:
1) not registered on the PC with a valid license or
2) The version is a pre-release version of EcoStruxure Machine Expert v1.0 which did not support this operation

Resolution
You will need to have an Activation ID provided in your purchase email or mailed paper copy (in the format: "A-XXXX-XXXX-XXXX")

Launch the Schneider Electric License Manager and check that the Name of the License row is either of the following:
1) EcoStruxure Machine Expert Standard
2) EcoStruxure Machine Expert Professional
and that the Version is 1.1
(this version number "1.1" in the License Manager is valid for both Machine Expert v1.1 or v1.2.x installed on the PC)

If those either of those do not appear, or the Version shows 1.0, follow the steps below to register by web:
  1. Start the Schneider Electric License Manager Tool
  2. In the Local tab click the Activate button.
    Result: The Activation ID dialog opens.
  3. Enter the Activation ID which can be found in the Entitlement Certificate of the software product to be activated.  If you want to activate multiple software products, you have to enter the different Activation IDs in separate lines.
    Result: The Next button is enabled.
  4. Click the Next button.
    Result: The Activation in Progress dialog opens.
    In the text box information about the internal processing of license activation is displayed.
  5. After the license is successfully created, click the Finish button.
    Result: The Local tab of the Schneider Electric License Manager is displayed showing each activated license in a new line.
To see your existing registered/floating licenses, visit:
https://www.se.com/sites/corporate/en/support/software-licensing/landing-page

Schneider Electric Việt Nam

Tìm hiểu thêm
Phạm vi:
Bài viết có thể hữu ích
Tìm hiểu thêm
Phạm vi: