What size panel (or range) does the NetShelter cage nut fit?
Issue:
The panel range for NetShelter cage nuts is requested.

Product Line:
NetShelter SX, SV, VX and WX hardware.

Environment:
AR8100, AR8005

Cause:
Extra cage nuts are needed and must be sourced locally.

Resolution:

The NetShelter cage nut panel range is 1.6mm - 2.0mm. This equated to a 14 awg to 16 awg panel.
All cage nuts provided by APC for NetShelter cabinets use this size, regardless of nut/screw combination.

Schneider Electric Việt Nam

Tìm hiểu thêm
Phạm vi:
Bài viết có thể hữu ích
Tìm hiểu thêm
Phạm vi: