Activation of alarm screens on Easergy P5 front display.
Can I configure alarm screens to be automatically activated after a trip?

Yes, alarm screens can be enabled/disabled from Easergy Pro.  They will appear directly on the front display of the device, and will continue to be displayed until the alarm has been acknowledged.

By default all Event alarms are enabled. But you can select individual Events through Easergy Pro to enable and disable the alarm screens.

Schneider Electric Việt Nam

Tìm hiểu thêm
Phạm vi:
Bài viết có thể hữu ích
Tìm hiểu thêm
Phạm vi: