Can the HMIGTUx be used with a normal HMIDT screen?

Article available in these languages: Tiếng Tây Ban Nha

Issue:
There is no information regarding if the HMIGTUx series is compatible with the HMIDT series screens and vice versa.

Product Line:
HMIGTUx, HMIGTU, HMIG3X, HMIG3U, HMIG5U, HMIG5U2

Resolution:
When using the HMIGTUx series (HMIG3X), it must be paired with an HMIDT35X, HMIDT65X, or a HMIDT75X. It is not possible to use HMIDT (non-extreme) with an HMIG3X. Vijeo Designer is not able to recognize this combination.

Similarily, it is not possible to use the HMIG3U, HMIG5U, HMIG5U2 with the HMIDTx (extreme) displays.

Schneider Electric Việt Nam

Tìm hiểu thêm
Phạm vi:
Tìm hiểu thêm
Phạm vi: