Can we access the fieldbus network of BMENOC0321 via its front ports?
  1. Issue
When ip forwarding service is activated, the BMENOC0321 makes its fieldbus network configurable and automatically enables its backplane port.
Then can we access(ping) the fieldbus network of BMENOC0321 via its front ports?
  1. Environment
N/A
  1. Resolution
No, the fieldbus network address is not accessible via BMENOC0321’s front ports.
It is only accessible via M580 or other Ethernet module(for ins. BMENOC0301) when the other module’s backplane port is enabled.

Schneider Electric Việt Nam

Tìm hiểu thêm
Phạm vi:
Bài viết có thể hữu ích
Tìm hiểu thêm
Phạm vi: