Can I use the ATV660 potentiometer in Hand and Auto?
Issue:
Can the drive be controlled in Hand or Auto only using the Potentiometer on the door?

Product Line:
Altivar Process Drive

Environment:
ALL

Cause:
Programming

Resolution:
You can use only the Potentiometer for speed control.
Go to My Preferences > Access Level and set to Expert
Go to Complete Settings > Command and Reference > Ref Freq Channel 1, change from AI3 to AI1.

Schneider Electric Việt Nam

Tìm hiểu thêm
Phạm vi:
Bài viết có thể hữu ích
Tìm hiểu thêm
Phạm vi: